STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1463 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 569 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! HAL_I2C_Mem_Read get stuck on the line

Hi,I am using NUCLEO stm32f030r8 to communicate with LIS3DH accelerometer, connection is in such a way thatvcc - 3v3GND - GNDSCL/D15 - SCLSDA/D14 - SDAI want to read from who iam i register 0x0F, we use sparkfun board hence we checked SDO pin is givi...

Midhun by Associate II
  • 2669 Views
  • 4 replies
  • 0 kudos

Receiving data from peak device to stm32f103c8t6 using can.

Hello STM32 community,I hope this message finds you well. I'm currently working on a project where I need to receive data from a Busmaster connected Peak device using a STM32F103C8T6 microcontroller via the CAN interface. I'm relatively new to CAN co...

AKZORO by Associate
  • 2796 Views
  • 3 replies
  • 1 kudos

DEV_TARGET_RESET_ERR

It is an STM32F103C8T6 chip, and I am trying to connect it using st-link v3.Connects to SWD,(Connected VCC, SWCLK, GND, SWDIO 4pin)In STM32CubeProgrammer, it is connected normally and both read/write are possible.However, it does not work when debugg...

TX_WAIT_FOREVER doesn't in debug

I have a board design using STM32H743.I am using:STM32CubeIDEVersion: 1.13.2Build: 18220_20230914_1601 (UTC) running on:OS Name Microsoft Windows 10 EnterpriseVersion 10.0.19045 Build 19045System Type x64-based PCI am debugging an implementation of A...

How to add a existing folder to STM32CubeIDE project?

Hi,I copy a folder from other project to the STM32CubeIDE project, then do right click and "Refresh", The project explorer will add the folder to the project. I also the new folder path to the project path via "property->c/c++ build->setting->toolcha...

zqizh.1 by Associate III
  • 22740 Views
  • 4 replies
  • 3 kudos

How long can SWV trace log with PC Sampling run?

Im running a debug on a STM32F413CHUx, I'm to figure out the cause of an IWDG reset. To help me I'm running SWV Trace Log outputting the PC Sampling at a cycles per sample of about 16,000 (the highest option).I increased the trace buffer size to 2000...

STM32CubeIDE

I have a project that I created using STM32CubeIDE. It was working fine then something glitched with the network and now it says the project file is corrupted and will not load. I have spent most of the day (should have done this earlier) trying to f...

HalC by Associate
  • 1438 Views
  • 1 replies
  • 1 kudos

Resolved! trash in hex file

Hi all!I have a project in STM32CudeIde that being downloaded via ST-Link works correctly. Also I have a hex file in MyProject/Release. If I compare downloaded via ST-Link code inside MCU with the hex file, they are different. So I cannot use the hex...

Rukki by Associate
  • 1963 Views
  • 2 replies
  • 1 kudos

Error occur

i am using stmcubeide and  make: *** [makefile:79: ADC 1.elf] Error 1 this error occur. please help me to resolve this. 

Pooja321 by Associate II
  • 2400 Views
  • 5 replies
  • 0 kudos