STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1477 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Change preprocessor values with headless build?

I'm trying to change a preprocessor value when building a project through the command line headless build.I can add a value through the command line using -D MY_VAL=10 which works fine if that value has not previously been defined. But I would like t...

Tom_y by Associate
  • 2552 Views
  • 3 replies
  • 1 kudos

Resolved! ADC + DMA stops reading

I have a setup which reads data from 4 step-motors and some sensors over ADC1(CH0, CH1, CH2, CH3), and ADC2(CH0, CH1). The system executes continuous ADC conversions in DMA Mode in the following way:- In the while-loop in the main function, it reads ...

GComes by Associate III
  • 3279 Views
  • 4 replies
  • 0 kudos

HardFault Debug in STM32CubeIDE

Some time ago, I was getting a Hardfault in a STM32F103 baremetal firmware. Even posted the question here, but I wasnt able to fix it. So, I moved to FreeRTOS-CMSIS, not to get rid of the problem, I was moving anyway. I'm still with this issue.I thin...

0690X00000BuhwiQAB.png
rrnicolay by Associate II
  • 14133 Views
  • 11 replies
  • 0 kudos

Resolved! CMSIS DSP and STM32CubeIDE

I hope you are doing well,So I've got a problem which its driving me crazy. I am trying to implement FIR filters in my stm32cubeide proyect by using CMSIS-DSP library, but I gess I am not importing the lib correctly or something, because everytime I ...

malatuni by Associate II
  • 6227 Views
  • 6 replies
  • 4 kudos

Resolved! How to change the Repository path in CubeIDE?

Hello community, I have a problem with new project creation, whenever I want to create a new project I come across this error: create minimal project failure: cannot read template source. reason: internal error i know the problem which is having a sp...

JBazm.1 by Associate III
  • 21923 Views
  • 12 replies
  • 6 kudos