STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1418 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

maintenance announcement

Dear community  our servers will be in maintenance Saturday 10th from 17h00 CET to 22h00, then you should have issues to login to our community or to our STM32Cube tools.  thanks for your understanding and don't hesitate to report any issues after th...

Interrupt mode for ADC reading does not work as expected.

hi,I would like to use HAL_ADC_Start_IT to let the ADC peripheral call interrupt whenever conversion is completed continously. Then I would like to print that converted value via UART.However, eventhough I select the continous conversion mode enabled...

demir by Senior II
  • 1407 Views
  • 0 replies
  • 0 kudos

Delete STM32 HAL/LL errors in clang-tidy

Hello, I am trying to integrate clang-tidy to a STM32 cmake project. But I am facing a lot of error from clang-tidy in STM32 HAL : error: use of undeclared identifier '__STREXW' [clang-diagnostic-error] error: cast from pointer to smaller type 'uint3...

Aahai.1 by Associate
  • 2104 Views
  • 1 replies
  • 0 kudos

Server problems

 I'm using the NUCLEO-L433RC-P board for the first time. I made a simple code for making a LED blink just to make the card output anything yet I keep getting two error messages. Precisely "Failed to execute MI command: target remote localhost:61234" ...

Mr4 by Associate III
  • 2860 Views
  • 4 replies
  • 0 kudos

Resolved! Flash binaries in STM32F7

Hi all,I have a project on a STM32F7 target and I work on STM32CubeIDE.How can I generate the binaries from the code ? And how can I flash the binaries in the STM32F7 (in NUCLEO-STM32F7ZG board) ?I don't want to use the "flash" button of the app, as ...

Remi99 by Associate II
  • 4032 Views
  • 3 replies
  • 3 kudos

SPI problem in STM32F446 NUCLEO

Hello everyone im currently working on a adc AD7708. I want to read chip from the device but i cant get any valid value. Here is the register sturucture of AD7708:I wrote a basic code to read the chip id from id register. Here is the code:      whil...

mrkayaalp_0-1707326670954.png mrkayaalp_1-1707327149557.png
mrkayaalp by Associate III
  • 6503 Views
  • 19 replies
  • 3 kudos

PA4/SPI_NSS, PA5/SPI1_CLK, PA6/SPI1_MISO

Hi,I have a problem with these pins PA4/SPI_NSS, PA5/SPI1_CLK, PA6/SPI1_MISO I programmed the chip so that those pins are a digital input to check for current present(no current = 0/current present = 1) this process carried out by connecting a wire.a...

rib.1 by Associate II
  • 2224 Views
  • 4 replies
  • 2 kudos

Issue in Input capture for overflow condition.

Good morning community,I am capturing the frequency using waveform generator in STM32.Board: STM32F401RE Nucleo.It is working at underflow condition.Condition is,Reference clock is 25MHz and counter period is 65535. So, minimum frequency is 382Hz and...

MG1 by Associate II
  • 2177 Views
  • 2 replies
  • 0 kudos

Resolved! ST-Link V2 Update Error

I can't update my ST-Link V2When i try to update first it says update error after that update succesfully. 

St link .png
AnilKose by Associate II
  • 2254 Views
  • 2 replies
  • 0 kudos