STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1405 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Facing Hard fault when implementing RTOS on NUCLEO-H563 board

Hi  I am trying to RTOS on my device STM32-H563ZI I get a hard fault when I hit the function osKernelStart(); in the main loop When I started debugging ,my code seems to get  hardfault after vStartFirstTask in function xPortStartScheduler() I am tryi...

Kendall7 by Associate II
  • 1550 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to configure Clock using baremetal PLL in stm32 G071RB

i tried to configure clock by writing code in its appropriate registers...following is the clock configuration function void SystemClockConfig(void){    #define PLLN  16 //using external clock sourceRCC->CR |= RCC_CR_HSEON;while(!(RCC->CR & RCC_CR_HS...

HZ by Associate II
  • 3389 Views
  • 4 replies
  • 2 kudos

Resolved! CubeIDE running incorrect version of firmware

Using the following version of Cube: Version: 1.14.1Build: 20064_20240111_1413 (UTC) We first changed the repository location for downloading packages. Then we manually downloaded the U5 package (why is this not available from the package manager?) a...

Eqqman by Associate III
  • 1486 Views
  • 2 replies
  • 0 kudos

Resolved! Error in STM32DMA.cpp, L8ClutLoaded not declared

Starting a new STM32F4 project I decided it would be a good idea to update all the development tools.  TouchGFX v 4.23.2STM32CubeMX v 6.11.0STMCubeIDE v 1.15.0 A working .ioc file from the previous project release was upgraded using the latest STM32C...

RLarr1_0-1711030381528.png RLarr1_1-1711030506241.png RLarr1_2-1711030558988.png RLarr1_3-1711030650112.png
RLarr.1 by Associate III
  • 3661 Views
  • 7 replies
  • 0 kudos

Some files popping up

Hi, I use CubeIDE 12 and compile and load my code with the the green and white 'run debug' button at the top. That works fine but at the end some file from the project pops up and the editor is focus away from the sourcefile to that file. Where/how c...

DetlefS by Senior
  • 2248 Views
  • 3 replies
  • 1 kudos