STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! external loader file not found

  I am using the STM32F429I board using the stmcubeIDE i tried to load the program via st-link but it got ended with the above program.After that i tried the alternate steps by loading the external loader but i cant find the (.stldr) file in the exte...

Muthamizh_1-1725608648684.png Muthamizh_0-1725608524755.png Muthamizh_3-1725608904172.png
Muthamizh by Associate II
  • 3533 Views
  • 4 replies
  • 0 kudos

Resolved! Turning ON onboard LED with Button Press

Hello, Am building a code on the NUCLEO-L4R5ZI-P to control motors on a robot. I want to include button presses to activate different modes (speeds, directions, etc). Setting ports as GPIO_Inputs and connecting and pressing the buttons is not working...

Odd_coder by Associate III
  • 7326 Views
  • 4 replies
  • 2 kudos

Resolved! Device configuration tool not working i cannot also set targeted project type to stm32cube but only to empty , have tryin several board types and cpu , after click "finish" the device configurator doesnt displaying nothing it is empty white window

I have tryin many versions of stm32cubeide + reinstalling them + also reinstalling windows 10 and still cannot get running device configuration tool inside ide etc..

Lfili.11 by Associate II
  • 11560 Views
  • 7 replies
  • 1 kudos

CubeIDE does not update touchgfx display

Any project I have tried to run from the CubeIDE will only display a static screen. I am using the STM32H7B3I-DK.I currently have my project setup to show one screen for a second and then switch to another that has wildcard values that update. The sc...

Resolved! USBx CDC ACM Dual Composite not working on STM32H723

Hello all, Following up on https://community.st.com/t5/stm32cubeide-mcus/usbx-dual-composite-cdc-acm-not-working/td-p/708277, I tried to implement the same Dual CDC-ACM on STM32H723 Nucleo. I have run into the same issues.With just one CDC_ACM class ...

NRedd2_0-1723621915432.png
NRedd.2 by Senior
  • 5106 Views
  • 7 replies
  • 2 kudos