STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1537 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 586 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Fail to perform local copy

I installed STM32CubeIDE 1.14.0 on Ubuntu 20.04.When trying to create new STM32 project by selecting 'Tx_CMSIS_Wrapper' for 'STM32F469I-DISCO' it seems to download everything needed but fail with message as subject line. 

PeterL by Associate III
  • 7791 Views
  • 10 replies
  • 3 kudos

Resolved! COMPILATION USING BATCH FILE

Can anyone help me to generate bin and hex file from source code using command prompt and batch file without stm32cubeide or its related any development environment?

arun27 by Associate II
  • 1787 Views
  • 3 replies
  • 1 kudos

Resolved! Unable to login to ST account in STM32CubeIDE

I downloaded the Version: 1.15.0 of STM32CubeIDE. It askes to login in ST for new project to download all the package. When I clicked on the myst -> login, "User Authentication Dialog" opens and nothing happens after that.Thus I am unable to login.Th...

Palak_0-1713545146411.png
Palak by Associate II
  • 6338 Views
  • 9 replies
  • 3 kudos

Resolved! With STM32Cube IDE v1.15.0 update problem with STLink

Hello all,I have updated the STM32Cube IDE version to the 1.15.0, it has own STLinkUpgrade tool which is also updated to version 3.14.5. But a problem arised. It wants me to update my STLink V2 firmware. When I tried, It gives error like:"Unexpected ...

mcagriaksoy_0-1710936591320.png mcagriaksoy_1-1710936651740.png

Resolved! Win11 - Failed to generate code CubeMX 6.13

Hi,CubeMX is unable to generate code. The program freezes and I find the following message in the logs. 2025-01-04 21:22:40,906 [INFO] BlockDiagram:2766 - set Specific Code input for plugin: RCC 2025-01-04 21:22:40,921 [INFO] CodeGenerator:896 - code...

p2baron by Associate II
  • 2881 Views
  • 5 replies
  • 3 kudos

Resolved! Facing issue while creating external flash loader

I am using NUCLEO-H563ZI evaluation board and i want to create external flash loader for IS25LP128 QSPI flash memory. I used external loader files from GIT HUB and .stldr file in STCUBE programmer external loader folder location. when i try to read f...

Nagarajan_2-1711548543593.png
Nagarajan by Associate III
  • 28115 Views
  • 54 replies
  • 6 kudos

CubeIDE opens random files on debug start / end

Since a while - I guess since update 1.8 or something - CubeIDE opens random project *.c-files, when the debug process is started or stopped.In this example only main.c was open. When I clicked on "debug", "startup_stm32_g473vetx.s" was openend, and ...

a.png
CBerg by Senior II
  • 5060 Views
  • 5 replies
  • 6 kudos