User Activity

I use Cube to setup TIM1_CH4 on PE14 as PWMSetup of iocPE14 -> TIM1_CH4 in pinoutTIM1:Ch 4 PWM Generation Ch4Conter Settings: Counter period 20PQM Generation Cannel 4: Pulse 5Modification of main:/* USER CODE BEGIN 2 */HAL_TIM_PWM_Start(&htim1, TIM_C...
I installed STM32CubeIDE 1.14.0 on Ubuntu 20.04.When trying to create new STM32 project by selecting 'Tx_CMSIS_Wrapper' for 'STM32F469I-DISCO' it seems to download everything needed but fail with message as subject line. 
When doing generating a project from STM32CubeMX (for F4 family) and converting it to a library in keil, then when keeping main in executable project and linking to library wrong implementation of *MspInit gets selected. The weak ones are selected ev...
Hi   When generating for CubeIDE firmware executes fine in both production and engineering mode. But for IAR/EWARM only engineering mode works. And, yes, I am aware of production mode not supported out of the box. Manual copy to target and start requ...
Error message: Updater cannot rename Software folder.... There is no other process locking it (procmon has no LockFile on Software).
Kudos given to