STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 242 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4083 Views
  • 0 replies
  • 3 kudos

stm32wb5mmg CPU2 do not go to sleep

Hello,I have an STM32WB5MMG chip, and I work with power consumption. I have the problem that after I stop advertising (aci_gap_set_non_discoverable()), I see that a flag LL_PWR_IsActiveFlag_C2DS() is still False, and I can not switch to Switch_On_HSI...

Vandr.1 by Associate II
  • 851 Views
  • 1 replies
  • 0 kudos

If you have open source FUOTA - Android and IOS

Hello everyoneI watched the video on ST's MOOC about how to integrate FUOTA via BLE for the STM32WB55 microcontroller and applied this Bootloader feature via the "ST BLE Sensor" smartphone app to the project of a product I'm developing and it's worki...

sibort50 by Associate II
  • 2047 Views
  • 5 replies
  • 1 kudos

X-NUCLEO-WB05KN CN7 cts/rts don't work

Hi I'm trying to connect NUCLEO-H755ZI-Q with X-NUCLEO-WB05KN via usart. I'm using usart2 (pd3, pd4, pd5, pd6) on the host board and CN7 on the shield. BLE initialisation fails if I set `hw-flow-control` in Zephyr in devicetree. Without flow control ...

dd1337 by Associate
  • 913 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WL LPUART1 for both Bootloader and AT Commands

Hello i Have a question about the STM32WL5MOC.I need to be able to use the bootlader of the WL and in the same UART line use the AT Command.But it seems that LPUART1 that is the only way to use AT Command Application is not used in the bootloader.Do ...

Hamady_0-1747983488598.png Hamady_1-1747983513094.png
Hamady by Senior
  • 2114 Views
  • 4 replies
  • 1 kudos