STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 230 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4073 Views
  • 0 replies
  • 3 kudos

STM32WB5MMG using it slave configuration

Hello All,I'm using STM32WB5MMG in my design, can anyone guide and share the schematic how this module can be used in slave configuration. This will help me to proceed in my design.Best Regards,Sakshi 

sakshi by Associate III
  • 899 Views
  • 3 replies
  • 0 kudos

stm32wb fifo bonding list

HII am on one of the latest stacks,  looking to make the bonding list a FIFO, need of some better understanding of your nvm for that. Q: Do you always add the new bonding key to the end of your nvm ? When I delete a bonding entry, does it shift other...

DS.4 by Senior II
  • 478 Views
  • 0 replies
  • 0 kudos

Resolved! Control of STM32WB55CG via BT Simple Terminal application

Hello, everyone,My project uses the WB55CGU6 microcontroller.The project is for me to be able to pair with the microcontroller via a phone app (e.g. BT Simple terminal) and use commands to control it. For example, if I send ‘1’ in ASCI on the phone a...

Procek by Associate
  • 768 Views
  • 1 replies
  • 1 kudos

Resolved! NUCLEO-L073RZ LoRaWAN end-node set up for TTN

I recently got the P-NUCLEO-LRWAN2 board. I'm trying to set up the end node NUCLEO L073RZ using STM32IDE. I want to flash the firmware to the end node, get response from it for AT commands in Tera Term and connect it to TTN. Please provide the step b...

Kaaviya by Associate II
  • 2701 Views
  • 8 replies
  • 0 kudos

Resolved! TrustZone Enable afterwards

Hi All,I wrote my code in STM32IDE without using TrustZone. Now I need to enable it, however this does not appear to be available in STM32IDE once the project has been created. Am I correct, or is it possible to enable TrustZone for an existing proje...

Cati by Associate
  • 1008 Views
  • 1 replies
  • 0 kudos

Resolved! Are all STM32WL55 packages comes with RF Shield

Hello ST Community,   Looking for the below details. I am new to ST Micro family. I came across the STM32WL55 and STM32WLE5 Chip set. Currently I have ordered STM32WL55JC1 nucleo board and STM32WLE5 seed studio wi-e5 development board. I am planning ...

Resolved! bt_enable() fails with Zephyr/nucleo-WB55RG

I try to initialize bt, with bt_enable() in zephyr. So far, no success,it returns me a -19 error ( not found )Any help would be very appreciated.Note: I am using Zephyr ( not Cube/HAL ).Context:- Zephyr 4.1.99- Board stm32 nucleo-wb55rg- FUS version ...