STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

B-L072Z-LRWAN1 is not recognize (COM port)

Posted on April 27, 2018 at 14:57Dear Community,I've bought 2 different evaluation boards to know better LoRa with STM32 MCUs. First, I bought the Nucleo board with the Mbed shied from Semtech ( P-NUCLEO-LRWAN1). I've managed to connect it to my lap...

STM32L072CZ Lora Keil License

Posted on May 04, 2018 at 13:54Hi,if I build the programm 'AT-Slave' (STMCubeExpansion_LRWAN) I got an License Error from Keil ( error: L6050U: The code size of this image (38072 bytes) exceeds the maximum allowed for this version of the linker.). I...

B-L072Z-LRWAN1 CN11 (USB Conn.) - Device mode

Posted on May 01, 2018 at 16:05Hi Everyone,I would like to ask a question regarding to powering the B-L072Z-LRWAN1 direct from the CN11 USB connector.The user manual of the B-L072Z-LRWAN1 states the following:''When the B-L072Z-LRWAN1 board is power...

Sigfox and LoRa on B-L072Z-LRWAN1

Posted on April 19, 2018 at 16:31Hello, I would like to know if someone ever experience to put Sigfox stack and LoRa stack (stack from St) at the same time on the murata module ? I would like to re initialize the hardware (HAL_Init( ), SystemClock_C...

Resolved! Current consumption using B-L072Z-LRWAN1

Posted on March 26, 2018 at 16:28Hi!I'm curently using the B-L072Z-LRWAN1 (STM32L072 and LoRa board) with the STM32CubeExpansion_LRWAN_V1.1.4, and i'm trying to reduce the current consumption using this board.I'm currently running into a high curren...

Resolved! I-CUBE-LRWAN: how to turn on continuous Tx mode

Posted on March 09, 2018 at 09:15Hello,I am using the I-CUBE-LRWAN V1.1.4 with CMWX1ZZABZ-078 and I want to test the continuous TX mode in order to check the EMC tests. Can somebody give some idea on how to do that?#continuous-tx #cmwx1zzabz-078 #i-...

algis by Associate II
  • 2468 Views
  • 3 replies
  • 0 kudos

Regarding SigFox stack for B-l072Z-LRWAN1

Posted on March 13, 2018 at 23:07Hi,I have b-l072Z-LRWAN1 + SigFox SDR dongle. I added Node's ID to SENK (network emulator), then I loaded AT command and push button examples from X-CUBE-SFOX, and nothing worked. When I sent a frame, it seems that s...