User Activity

Hello Community,i have followed the documentation on how to enable RDP-like product state flash protection in STM32H5 microcontrollers.https://community.st.com/t5/stm32-mcus/how-to-enable-rdp-like-product-state-flash-protection-in-stm32h5/ta-p/708082...
Hello Community,I have few "Buttons with Labels" within a scroll list where I am able to scroll within the scroll list using a hardware button and animateToItem function.What I would also like to do is to show which Button with label is active.Is the...
Hello Community,I have an incremental encoder with 30 detents interfaced on STM32H5562 where I have set my TIMER2 in Encoder mode  and using interrupt as shown below: static void MX_TIM2_Init(void){ /* USER CODE BEGIN TIM2_Init 0 */ /* USER CODE END ...
Hello Everyone,Is there any plan for ST to provide support drivers for the MX25L6433F serial NOR flash on the STM32H5 series of micros?MX25L6433F is the flash used on the X-NUCLEO-GFX01M2.Thanks. 
Posted on May 01, 2018 at 16:05Hi Everyone,I would like to ask a question regarding to powering the B-L072Z-LRWAN1 direct from the CN11 USB connector.The user manual of the B-L072Z-LRWAN1 states the following:''When the B-L072Z-LRWAN1 board is power...