cancel
Showing results for 
Search instead for 
Did you mean: 

Having problem with B-L072Z-LRWAN1, when I try to program this device with stm32cubeprogrammer I found the following programming problem (connection with ST-LINK) corrupted database I have more board with this problems....

csard
Associate II

Error: ST-LINK error (DEV_TARGET_CMD_ERR)

Error: Device not supported

flash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0x0.stldr is loaded

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Try some different cables.

Make sure the ST-LINK firmware is updated to current.

Change connection options, or create the test/debug builds without the lower power entry (turns off the scan chains being used to program/connect)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
csard
Associate II

how change the connection option and send program to the board?