cancel
Showing results for 
Search instead for 
Did you mean: 

Hello everyone, I am trying to flash ble stack into CM0 processor because I suppose I erased the entire memory by mistake using stlink programmer, but I have some problems.

RNoga
Associate

The answer from the processor is

RSS state is WIRELESS_STACK_UPGRADE_ONGOING

RSS status is RSS_IMAGE_NOT_FOUND

RSS state is RSS_IDLE

RSS status is RSS_NO_ERROR

Firmware Upgrade process started ...

Updating firmware ...

Firmware update finished

Firmware Upgrade command execution finished

I tryed with all the software (server, client ecc.) but it doesn't work.

What I do not understand is that in help description it is said that file name and address are optional in fwupgrade command. How is it possible ? If I do not specify the binary file with the stack, how can it flash inside the micro ? Maybe they are silly questions, but I do not really understand where I am wrong. Thank you very much for helping me.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0