STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 234 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4077 Views
  • 0 replies
  • 3 kudos

Resolved! Should I Download All Wireless Stacks?

Hi,expert.I am a beginner who started using STM32WB.I am trying to download the wireless stack using STM32_ProgrammerCLI.exe and command prompt while reading UM2550.I understand that there are seven types of wireless stacks:・stm32wb5x_BLE_Stack_fw.bi...

ota-s by Associate II
  • 1562 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to understand TSC connections in STM32WB

Hi Sir/Madam,The Sensor Capacitor (Cx) is not connected in the below mentioned. Can you please provide clarity on the Cx connection with MCU.While configuring the shielding in TSC using STM32CubeMX, it is asking to configure Cs(Sampling Capacitor) in...

0690X000009YxMyQAK.jpg 0690X000009YxP9QAK.png
GShai by Associate II
  • 2649 Views
  • 5 replies
  • 1 kudos

LORA End_Node

hello, Please be kind to me as I am new to this. I have a B-L072Z board.Use the End_Node program to communicate with the lora gateway, I found that the data transmission interval of the terminal is 10 seconds. I can reduce the time to 7 seco...

Yxiao by Associate
  • 667 Views
  • 0 replies
  • 0 kudos

Migrate from expansion boards to anothere

Hi, I want to use i-cube lrwan stack for my hardware, I use stm32l151cb+sx1276. I have tried to use STM32L152RE-Nucleo and modify it. I did it for the microcontroller side and have modified pin and peripherals mapping. but I can't change radio expans...

Iot_king by Associate
  • 1840 Views
  • 3 replies
  • 0 kudos

multiple power supplies

Hi Sir/MadamIn MB1355 MCU supply domain schematics(above one) I didn't understand supply connections. If only 3V3 supply given which connections are not required in the schematics?

0690X000009Yu5kQAC.png
Anitha by Associate III
  • 2739 Views
  • 9 replies
  • 1 kudos

STM32WB55 BLE OTA Code Size with SW4STM32

Hey,I'm trying to get a binary for the BLE OTA application, but if I compile the example BLE_Ota with SW4STM32 the binary is around 393.411 KB. STM32CubeWB 1.1.0 with Patch 1.1.1 was used.How can I get the same size and file type like the reference f...

benny by Associate II
  • 1014 Views
  • 0 replies
  • 0 kudos