User Activity

Hey,I'm trying to get a binary for the BLE OTA application, but if I compile the example BLE_Ota with SW4STM32 the binary is around 393.411 KB. STM32CubeWB 1.1.0 with Patch 1.1.1 was used.How can I get the same size and file type like the reference f...
Posted on July 11, 2018 at 20:25Hi,I have a B-L475E-IOT01A2 board and problems with the Wifi example.I have assembled the missing parts for the HSE (8 MHz crytsal) and everything works fine with the USB Host (MSC) example. I also tested all the sens...
Posted on June 26, 2017 at 16:03Hey,I have a problem with the I2C1 on the STM32F746G-Discovery.I'm using the example-code for communication with DMA, but I changed the address mode from 10bit to 7bit.Now it's getting strange. The ST-Board is the mas...
Posted on June 19, 2016 at 01:46 Hi, I want to ask if someone can confirm that the STM32F769I-DISCO has a high-pitched https://www.dict.cc/englisch-deutsch/buzzing.html https://www.dict.cc/englisch-deutsch/sound.html. I think it's from th...
Posted on August 24, 2015 at 13:51Hi all,I have a question about the different memory sections. I use a modified version of the demonstration project.There are 4 memory sections:SRAMSDRAMFlashNOR (QSPI)This code save the variable to NOR:#if defined ...