STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 223 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

I keep getting an error with some of the example projects where files cannot be found when they do exist in the folder structure for the project and are pointed to in Atollic's (9.3) directory build reference.

Specifically, I am trying to compile the STM32WB Dongle Thread General CoAP example. Although this isn't a problem specific to STM32 but more with the IDE, I was hoping somebody might have a hint on how to solve the issue. Also, all of the files exis...

BLE Basics

Hi,I'm using STM32WB55 controller in my project for low power BLE. But I have zero knowledge on BLE. Can any one help me in understanding from basics of BLE.

RJ1 by Associate
  • 1172 Views
  • 1 replies
  • 0 kudos

IOT Project

Hlw Sir,I am piyush kumar having a STM32F030 Nucleo Board and one ESP8266 WIFI Module.I am very new to IOT . Can you please guide me on this how can i start IOT with these two.

PKuma.6 by Associate II
  • 859 Views
  • 0 replies
  • 0 kudos

How get timestamp in i.cube.lrwan library?

Hello, i have two b-l072z board and making LoRa comm as point to point. While I sending ADC data I want to add packet to timestamp. I have inspected hw_rtc.c file and find HW_RTC_GetCalenderValue function. But it make me confusing because of static...

Resolved! LPTIM PWM and Interrupt Issues

I am having problems running LPTIM1 off the LSE. When I set up and interrupt it is firing ever clock cycle and does not seem to be clearing. RCC_BDCR_LSERDY bit is active before selecting the LPTIM1 clock source. I have also tried disabling the inter...

Daniel L by Associate III
  • 3087 Views
  • 2 replies
  • 0 kudos