NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have an STM32WB55 Nucleo Pack and I am trying to set it up with my machine (Ubuntu 18.04.3 LTS) to run some sample code.I installed Atolic TrueStudio (version 9.3.0) and downloaded a sample project called "STM32100E-EVAL_USART_IrDA_Transmit". The p...
Is there an EEPROM emulation for STM32WB55CG as it exists for the STM32L476RG ?
HiI thinking of buying and STM32WB (P-NUCLEO-WB55 evaluation board) because of the fast ADC. I need to sample four analog signals with a rate of a few hunderd Ksps and store their values.what would roughly be the sample rate when using 4 adc inputs (...
Hello, I'm facing a strange problem. I just bought the LRWAN2 package, connected the gateway to the network, one usb cable to power it and one usb to the st-link. I configured the packed forwarder to router.eu.thethings.network,1700,1700 and CH to U...
I have TrueStudio v9.3.0, Stm32CubeProgrammer v2.0.0 and cubeMX ver5.2.0 installed. I can open and compile the hand-on project of BLE_HeartRate on TrueStudio but can't debug it. console shows: "Target no device found", error in initializing ST-link d...
I'm trying to perform I2C read from external EEPROM upon characteristic value change.I'm able to read from EEPROM before advertisement stage.I'm using sequencer to put char_value_handler in the main thread.But HAL_I2C_Mem_Read() returns HAL_ERROR.The...
Hello,I'm testing a custom board implementing a BLE Server. The binary for CPU2 is the stm32wb5x_BLE_Stack_fw 1.3.0. All the radio system seem work well, tested with STM32CubeMonitor-RF and a nucleo dongle (Packet Error Test below 1%). The advertisin...
Hi, I am trying to calculate the current consumption for my BL072z board1.- my formula:16mA in run mode30uA in stop modeT to tx data = 20 secsNumber of txs in a hour = 3600/20 = 180duration of each tx = 3 secondstotal TX time = 3(180)=540 seconds = 0...
Hello,i'm trying to send data to a server thanks to b-l072z-lrwan1 discovery kit but i can't even start the connexion between them.Here are the parameters that i've set/chosen on the server :here is the device parameter according server point of view...