STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 235 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4077 Views
  • 0 replies
  • 3 kudos

Resolved! Hi I'm using STM32CubeIDE for my nucleol476rg board. I'm trying to compile the I-cube-lrwan stack with the Cube IDE. Currently, after compiling I'm getting an error - command-line>:0:1: error: macro names must be identifiers . Please help.

These are my error messages - <command-line>:0:1: error: macro names must be identifiers<command-line>:0:1: error: macro names must be identifiers<command-line>:0:1: error: macro names must be identifiers<command-line>:0:1: error: macro names must be...

MAust.1 by Associate II
  • 4478 Views
  • 4 replies
  • 0 kudos

Trying to get the advertising state

Hello,I'm trying to get the advertising state from a new Cube MX project.I followed the step by step, did all the initializations and compare with the P2Pserver exemple.Everythings seem to be ok but I can't get this state work.It seems that the prog...

LVent by Associate II
  • 3754 Views
  • 7 replies
  • 0 kudos

Resolved! Unable to wakeup from WKUPx when UTIL_SEQ_Run is executed.

Good DayI am programming a stm32wb55rg to start upDo some ADC samplingStart up BLE using    APPE_Init(); Load all values in characteristic.And then i sit in loop running:UTIL_SEQ_Run( UTIL_SEQ_DEFAULT );After 60 seconds I put device in standby mode. ...

HSpre.1 by Associate III
  • 4625 Views
  • 8 replies
  • 0 kudos

Resolved! What does STM32WB offer that other modules don't?

I need to select a chip that offers me a BLE 5.0. What is the advantage of using STM32WB chips, rather than using other modules like Telit, Ebyte etc. Okay STM32 has CubeMX and easy implementation just as said in application notes, workshops etc. but...

y.arikok by Associate II
  • 1911 Views
  • 2 replies
  • 0 kudos

STM32WB(Nucleo board) cannot connect to STM32CubeProgrammer. STM32CubeProgrammer indicated "10:44:57 : ST-LINK error (DEV_CONNECT_ERR)".

Hello,NUCLEO-WB55 cannot connect to STM32CubeProgrammer. But STM32CubeProgrammer found ST-LINK. And I could upgrade ST-LINK Firmware. STM32CubeProgrammer indicated "10:44:57 : ST-LINK error (DEV_CONNECT_ERR)".Please check attachment image.Please let ...