User Activity

Is it possible to receive data from USB camera that is connected to the STM32 somehow? What is needed to implement it?Thanks.
I need to select a chip that offers me a BLE 5.0. What is the advantage of using STM32WB chips, rather than using other modules like Telit, Ebyte etc. Okay STM32 has CubeMX and easy implementation just as said in application notes, workshops etc. but...
I'm completely new to the embedded software and want to use STM32WB for my project, which will send image data from USART camera to the mobile phone. For now, I'm researching about BLE (protocols, characteristics etc.) and have no clue about how to u...
I'm currently receiving image data from TTL camera and sending it via Bluetooth. Baud rates for camera (VC0703) and Bluetooth module (HC-06) are 115200 and 230400, respectively. I'm defining camera rx buffer size and Bluetooth tx buffer size as 60000...
There are plenty of codes about VC0706 camera + Arduino. I tried the sample on Arduino and it worked pretty well. But I need to make this project with STM32. Any ideas how to implement and code VC0706 with STM32?