cancel
Showing results for 
Search instead for 
Did you mean: 

Hi I'm using STM32CubeIDE for my nucleol476rg board. I'm trying to compile the I-cube-lrwan stack with the Cube IDE. Currently, after compiling I'm getting an error - command-line>:0:1: error: macro names must be identifiers . Please help.

MAust.1
Associate II

These are my error messages -

<command-line>:0:1: error: macro names must be identifiers

<command-line>:0:1: error: macro names must be identifiers

<command-line>:0:1: error: macro names must be identifiers

<command-line>:0:1: error: macro names must be identifiers

make: *** [Utilities/subdir.mk:35: Utilities/queue.o] Error 1

make: *** Waiting for unfinished jobs....

make: *** [Utilities/subdir.mk:33: Utilities/low_power_manager.o] Error 1

make: *** [sx126x/subdir.mk:23: sx126x/sx126x.o] Error 1

make: *** [sx126x/subdir.mk:21: sx126x/radio.o] Error 1

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MAust.1
Associate II

I could solve it.

The additional '#' in -D#ARM_MATH_CM4 was the error

Thanks Clive for responding

View solution in original post

4 REPLIES 4

Look at the command line you're passing to the tools, perhaps the command line defines

Perhaps attach a project file, or the make file

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for responding!! Please find the makefile below -

################################################################################

# Automatically-generated file. Do not edit!

################################################################################

-include ../makefile.init

RM := rm -rf

# All of the sources participating in the build are defined here

-include sources.mk

-include sx126x/subdir.mk

-include Utilities/subdir.mk

-include STM32L4xx_Nucleo/subdir.mk

-include Mac/region/subdir.mk

-include Mac/subdir.mk

-include Drivers/STM32L4xx_HAL_Driver/Src/subdir.mk

-include Crypto/subdir.mk

-include Core/Startup/subdir.mk

-include Core/Src/subdir.mk

-include Basic/subdir.mk

-include Appsrc/subdir.mk

-include subdir.mk

-include objects.mk

ifneq ($(MAKECMDGOALS),clean)

ifneq ($(strip $(C_DEPS)),)

-include $(C_DEPS)

endif

endif

-include ../makefile.defs

# Add inputs and outputs from these tool invocations to the build variables 

EXECUTABLES += \

LoRa_Test.elf \

SIZE_OUTPUT += \

default.size.stdout \

OBJDUMP_LIST += \

LoRa_Test.list \

OBJCOPY_BIN += \

LoRa_Test.bin \

# All Target

all: LoRa_Test.elf secondary-outputs

# Tool invocations

LoRa_Test.elf: $(OBJS) $(USER_OBJS) C:\Users\alber\STM32CubeIDE\workspace_1.3.0\LoRa_Test\STM32L476RGTX_FLASH.ld

arm-none-eabi-gcc -o "LoRa_Test.elf" @"objects.list" $(USER_OBJS) $(LIBS) -mcpu=cortex-m4 -T"C:\Users\alber\STM32CubeIDE\workspace_1.3.0\LoRa_Test\STM32L476RGTX_FLASH.ld" --specs=nosys.specs -Wl,-Map="LoRa_Test.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group

@echo 'Finished building target: $@'

@echo ' '

default.size.stdout: $(EXECUTABLES)

arm-none-eabi-size $(EXECUTABLES)

@echo 'Finished building: $@'

@echo ' '

LoRa_Test.list: $(EXECUTABLES)

arm-none-eabi-objdump -h -S $(EXECUTABLES) > "LoRa_Test.list"

@echo 'Finished building: $@'

@echo ' '

LoRa_Test.bin: $(EXECUTABLES)

arm-none-eabi-objcopy -O binary $(EXECUTABLES) "LoRa_Test.bin"

@echo 'Finished building: $@'

@echo ' '

# Other Targets

clean:

-$(RM) *

-@echo ' '

secondary-outputs: $(SIZE_OUTPUT) $(OBJDUMP_LIST) $(OBJCOPY_BIN)

.PHONY: all clean dependents

.SECONDARY:

-include ../makefile.targets

Error for the makefile below -

################################################################################

# Automatically-generated file. Do not edit!

################################################################################

# Add inputs and outputs from these tool invocations to the build variables 

C_SRCS += \

C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/BSP/Components/sx126x/radio.c \

C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/BSP/Components/sx126x/sx126x.c 

OBJS += \

./sx126x/radio.o \

./sx126x/sx126x.o 

C_DEPS += \

./sx126x/radio.d \

./sx126x/sx126x.d 

# Each subdirectory must supply rules for building sources it contributes

sx126x/radio.o: C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/BSP/Components/sx126x/radio.c

arm-none-eabi-gcc "$<" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32L476xx -DDEBUG -DREGION_IN865 -DUSE_STM32L47XX_NUCLEO -D#ARM_MATH_CM4 -c -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Projects/STM32L476RG-Nucleo/Applications/LoRa/End_Node/Core/inc" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Projects/STM32L476RG-Nucleo/Applications/LoRa/End_Node/LoRaWAN/App/inc" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/CMSIS/Device/ST/STM32L4xx/Include" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/BSP/STM32L4xx_Nucleo" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/STM32L4xx_HAL_Driver/Inc" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/CMSIS/Include" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Crypto" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Mac" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Phy" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Utilities" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Patterns/Basic" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/BSP/Components/sx126x" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Projects/STM32L476RG-Nucleo/Applications/LoRa/End_Node/LoRaWAN/App/src" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"sx126x/radio.d" -MT"$@" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "$@"

sx126x/sx126x.o: C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/BSP/Components/sx126x/sx126x.c

arm-none-eabi-gcc "$<" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32L476xx -DDEBUG -DREGION_IN865 -DUSE_STM32L47XX_NUCLEO -D#ARM_MATH_CM4 -c -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Projects/STM32L476RG-Nucleo/Applications/LoRa/End_Node/Core/inc" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Projects/STM32L476RG-Nucleo/Applications/LoRa/End_Node/LoRaWAN/App/inc" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/CMSIS/Device/ST/STM32L4xx/Include" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/BSP/STM32L4xx_Nucleo" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/STM32L4xx_HAL_Driver/Inc" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/CMSIS/Include" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Crypto" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Mac" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Phy" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Utilities" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Middlewares/Third_Party/LoRaWAN/Patterns/Basic" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Drivers/BSP/Components/sx126x" -I"C:/Users/alber/Documents/LoRa/en.i-cube_lrwan/STM32CubeExpansion_LRWAN_V1.3.1/Projects/STM32L476RG-Nucleo/Applications/LoRa/End_Node/LoRaWAN/App/src" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"sx126x/sx126x.d" -MT"$@" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "$@"

MAust.1
Associate II

I could solve it.

The additional '#' in -D#ARM_MATH_CM4 was the error

Thanks Clive for responding