STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

I'm running the IEE802.5.4 protocol stack on the STM32WB50. Why does the System Clock Mtu source switch on its own?

HelloWe are verifying the communication of the IEEE802.15.4 protocol stack with STM32WB50. I tried to insert a 1ms interrupt on CPU1, but when I initialized and enabled IEEE802.15.4, the 1ms interrupt was extended to 2ms. The cause was that the Syste...

MNitt.1 by Associate II
  • 857 Views
  • 1 replies
  • 0 kudos

STM32L476RET6 + SX1262 (Ebyte E22)

Hello everyone,it seems like it is very hard to get an answer in any lora issues. I give it a shot anyway :DI've watched all the lectures in udemy to get familar with stm32 MCU and i have learned a lot, but unfortunately not enough to get a LoRa-Nod...

VNold.1 by Associate II
  • 8225 Views
  • 7 replies
  • 0 kudos

STM32F103 with LoRa (I-CUBE-LRWAN)

I currently have a NUCLEO-F103RB board and also an I-NUCLEO-LRWAN1 board.Is it possible to interface them directly together? I have seen that the I-NUCLEO-LRWAN is initialized for the STM32L0/L1/L4 series using the I-CUBE-LRWAN.However, I would reall...

MChar.1 by Associate II
  • 3487 Views
  • 5 replies
  • 0 kudos

STM32WLE5 documentation, cube package and evaluation board

Hello,I recently saw the new SoC STM32WLE5 which has been developed. Is an evaluation board available? Is there also minimal support (Cube package, documentation) to start development. I read in a document that there is a NUCLEO-WL55JC, but I couldn'...

MChar.1 by Associate II
  • 2611 Views
  • 4 replies
  • 0 kudos

How to update FUS trough OTA

Hello there !When I use Monitor RF to upgrade firmware(0x7000 offset on CPU1) and wireless stack (0xF000 offset on CPU2) trough OTA : It works.But when I want to upgrade (or just rewrite the same version of FUS) trough OTA at 0xF000 on CPU2 : it does...

DMatt.1 by Associate II
  • 1521 Views
  • 3 replies
  • 0 kudos

FUS_STATE_ERR_UNKNOWN || STM32WB50 Firmware update error

Attempting to update STM32WB50 Firmware using STM32 Cube Programmer in Boot mode (Boot0 pin connected to VDD)download stm32wb5x_FUS_fw_1_0_2 - Start Address 0x080EC000download stm32wb5x_FUS_fw - Start Address 0x080EC000download stm32wb5x_BLE_Stack_...

Aishwarya by Associate III
  • 1210 Views
  • 0 replies
  • 1 kudos