STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! What antenna filter can I use with STM32WB55 using BLE

Hello,I use a STM32WB55RGV7 microcontroller. Doing the hardware layout I'm confused about the antenna filter: - I can't get the band pass filter LFB182G45CGFD436 in small quantities, which is used in the P-Nucleo-WB55 - the low pass filter LFL212G45T...

HLenk.1 by Associate
  • 1983 Views
  • 2 replies
  • 1 kudos

System Timebase Source problem with STM32WLE5C8Ux

I have a custom hardware with an STM32WLE5C8Ux and I want to add functionality to it step by step. I'm using CubeMx to generate a project with success ,toggeling a GPIO works. I have not initalized external TCXO or LSE, they are populated but I want ...

MAebl by Associate
  • 3156 Views
  • 3 replies
  • 1 kudos

Availability of STM32WL55 WLCSP59-Package

Hi!I can't find the WLCSP59-Package at distributors like digi-key, mouser etc. It doesn't seem to be available. Does anyone know why?Is this a matter of time (not in mass production yet) or a matter of volume (only sold to specific customers)?If the ...

ABerg.4 by Associate
  • 881 Views
  • 0 replies
  • 0 kudos

What is the minimum supply voltage VDD for STM32WL family?

I read some contradictory information and I am not sure what is true. According to the document https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=&ved=2ahUKEwjX3NCZvoDwAhVIY8AKHe2zCrkQFjAAegQICBAD&url=https%3A%2F%2Fwww.st.com%2Fcontent%2F...

MAebl by Associate
  • 1120 Views
  • 0 replies
  • 0 kudos

Why examlpe "HandsOn_2" from STM32WB_workshop doesn't work?

I am trying to do the example "HandsOn_2" from STM32WB_workshop. Executes commands as described. The only difference is I use STM32Cube_FW_WB_V1.3.0 instead of STM32Cube_FW_WB_V1.0.0.STM32Cubex does not copy the scheduler.c, scheduler.h files to the ...

0690X00000Buey7QAB.png 0690X00000BuemkQAB.png
POlcz by Associate III
  • 2694 Views
  • 5 replies
  • 1 kudos

I want to reset and reinitialize only CPU2 (M0 +) of STM32WB

I want to reset and reinitialize only CPU2 (M0 +) of STM32WB I used to ask a question in "Data reception stops at Mac_802_15_4_FFD in the sample code."Even now, this matter has not been resolved.At the end, it was said that RFD was used, but since I ...

MNitt.1 by Associate II
  • 1039 Views
  • 1 replies
  • 0 kudos

STM32WB55 Unable to build p2p_Server sample application

Environment:MacOS 10.14.6STM32CubeIDE 1.6.1STM32WB SDK 1.11.0Starting with a clean install of Cube, SDK, empty workspace. Importing p2p_Server project (from the initial splash screen->Import STM32 sample app), the build fails with (among other):/Use...

ACoad.1 by Associate II
  • 712 Views
  • 0 replies
  • 0 kudos

Resolved! FP-AUD-BVLINKWB1

In the pack FP-AUD-BVLINKWB1, BLE audio streaming example provided with Opus codec, will you be also providing similar example using new LE audio standard with LC3 codec?