User Activity

I have soldered up my first STM32WLE5CCU6 project board, and it buzzed out nicely before I gave it power. Now VDD is permanently shorted to ground...I'm happy to try again, but: what is the minimum number of pins/components that I need to connect jus...
I think I'm misunderstanding something with the generic SPI transmit procedure. I'm working with the STM32L432, but I think that's the standard SPI device for most MCUs. My scenario is with the MCU as Controller rather than Peripheral...My issue is w...
Further to my previous question on the STM32L432KC at https://community.st.com/s/question/0D50X0000BAFA5fSQH/what-is-the-difference-between-these-two-clock-configurationsI am successfully increasing the clock rate from the reset rate of 4MHz to my de...
I am reading the STM32Lxxxx Reference manual (RM0394 Rev 4, October 2018, DM00151940).On page 267, section 8.4 "GPIO registers" says "The peripheral registers can be written in word, half word or byte mode." Sure enough, any access works.On page 308,...
Kudos from