STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! BLE low power mode advertising

I have one more confusion regarding BLE connection.For the case in low power mode,If device is already paired and connection is established, do we need to continuously advertise packets at regular intervals for connection to keep intact and to provid...

GMacw.1 by Associate II
  • 1147 Views
  • 1 replies
  • 0 kudos

stm32wb55cc code licensing

Hello. I create new empty project for stm32wb55CC in CubeIDE 1.6.1 with pack 1.11.0. main.c contains/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @br...

Resolved! Why CubeMonitor-RF(MRF) can't connect to my USB Dongle(STM32WB55CGU6) Virtual COM? MRF does display COM11 when I connect USB Dongle, but when I press CONNECT I get "Could not open COM port". Thanks in advance 4 help!

My dongle has latest FUS 1.1.2 and then programmed with stm32wb5x_Phy_802_15_4_fw.bin to proper address(0x080DE000) and with option "Start Wireless Stack" selected. 

DFOGE.1 by Associate
  • 1499 Views
  • 1 replies
  • 0 kudos

aci_gatt_update_char_value never returns

I am trying to send a BLE notification after I have connected. I add the characteristic this way. retVal = aci_gatt_add_char(serviceHandle, UUID_TYPE_128, (const Char_UUID_t *)Uuid, ...

BStic.1 by Associate II
  • 1288 Views
  • 1 replies
  • 0 kudos

STM32WLE5 STOP2 - Very High Current Consumption

I have a board with an STM32WLE5CC and am attempting to use STOP2 mode, but instead of the expected 4-6uA I am seeing 1mA consumption.All peripherals except FLASH, HSEM, and the RTC are disabled in the RCC block. All Unused GPIO are set to Analogue. ...

DMial.1 by Associate
  • 1449 Views
  • 1 replies
  • 0 kudos

Core Locked up on P-Nucleo-WB55 main board.

I have followed instructions from many threads but none seems to work. I am not sure if I tweaked the Anti-Rollback before a FUS update. Please help.So is there a way to revive my board ??If I have bricked my board and cannot REVERT back I need to k...

sougata by Associate II
  • 3675 Views
  • 5 replies
  • 0 kudos

Resolved! Can 'ST-LINK V2' be used in 'DISCO-L072CZ-LRWAN1'?

Development Environment: KEIL (Free License)보드 : DISCO-L072CZ-LRWAN1HelloTo build a monitoring system with the LoRa protocol now.It is being developed as a 'DISCO-L072CZ-LRWAN1' board.I turned off the 'ST-LINK' built into the board to check the min...

SYun.2 by Associate III
  • 1609 Views
  • 3 replies
  • 0 kudos