STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Not Receiving UART message from STM32WL5M to Laptop

Hi there, I have an B-WL5M-SUBG1 evaluation board which uses the STM32WL5M module.I am having problems with the STM32 receiving a message I am sending it from my laptop via python. I connect between the stm32 and the laptop via an RS422/485 converter...

Dicko by Associate II
  • 18880 Views
  • 27 replies
  • 1 kudos

Resolved! Update FUS to version 2.0.0 and BLE Stack via FOTA

Hi,We are using the STM32WB5 series. We have implemented a FOTA mechanism to update the BLE Stack and the FUS (both separately).We have noticed a new version of the FUS (2.0.0), which, to our understanding, is not backward compatible with older versi...

Novodes by Associate
  • 579 Views
  • 1 replies
  • 0 kudos

STM32WB09 Deepsleep mode with BLE

Hi,I want to create device, based on STM32WB09, with BLE and battery power. I get sample from CUBE and turn on CFG_FULL_LOW_POWER and CFG_LPM_SUPPORTED. It works, between BLE events MCU work in Deepsleep mode, but i need scheduller:1) Deepsleep2) wak...

Yevhen by Associate II
  • 717 Views
  • 3 replies
  • 0 kudos

Resolved! STM32WB35: LPUART1 Consuming around 4mA in STOP1 mode

I'm developing an application where I need to have both USART1 and LPUART1 configured to receive commands. I'm using STOP1 mode to ensure the commands can be received by both peripherals (USART1 will not work with STOP2 mode from my understanding). I...

LwtRuben by Associate II
  • 754 Views
  • 2 replies
  • 0 kudos