2021-04-08 5:42 AM
Namaste from India.
I am working on STM32WB Nucleo board for BLE functionality as per the tutorial available: https://www.youtube.com/watch?v=zNfIGh30kSs
I have copied the codes from workshop snippets provided by ST. When I press the LED on the ST BLE sensor App, the LED of the Nucleo board toggles its state. When I press the button switch 1, the notification is not received in the BLE app. The LED stops blinking and debugger shows this message: SIGTRAP:Trace/breakpoint trap) HardFault_Handler()
When I use the p2pServer project provided by the ST, it works flawlessly. If I build the project from scratch by following the tutorial, I am facing this issue.
Cube IDE Version: 1.6.1
CubeMX version: 6.1.1
STM32Cube_FW_WB_V1.10.0
Anyone here should help me.
Regards
Raghavendra
2021-04-11 5:14 AM
Hi,
I found the issue with the RegTask. Shifting was misisng in the code snippet provided by ST.
In p2p_serve_app.c in line 43:
UTIL_SEQ_RegTask( CFG_TASK_SW1_BUTTON_PUSHED_ID,0,P2PS_Send_Notification );
this must be
UTIL_SEQ_RegTask( 1<<CFG_TASK_SW1_BUTTON_PUSHED_ID,0,P2PS_Send_Notification );
This might help someone like me who took one week to fix it.
Thanks