NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I try to start a a continuous waveform (CW) from the STM32WB radio using theaci_hal_tone_start command from the DTM suite. I execute the following commands:hci_reset( );HAL_Delay( 10 );aci_hal_set_tx_power_level( 1, tx_pow );aci_hal_tone_start( R...
* JLink Info: Device "STM32WB55VG" selected.JLink info:------------DLL: V7.66d, compiled Jun 21 2022 17:00:22Firmware: J-Link Ultra V4 compiled Sep 24 2021 16:41:09Hardware: V4.00Feature(s) : RDI, FlashBP, FlashDL, JFlash, GDB * JLink Info: Found SW-...
Hi,For stm32wb flash operations we have to implement diagram described in AN5289, page 36. How about option bytes access? Do we have apply the same approach, with semaphores etc? Or we just can use regular HAL functions? Best,Mateusz
My expectation was that a pin-interrupt using EXTI will lead to wakeup times just slightly longer than the wakeup delays named in the datasheet (below 10µs), but what I see is this (falling edge on yellow finally reached the ISR on the magenta rising...
I am having similar issues with STM32WL54 with boot pin pulled up to 3.3V, it was initially working but suddenly stopped responding. I have tried connecting via a STLink using CubeProgrammer c2.12.0 and STLink Utility v4.6.0.0. Additionally, I have a...
Hello,I have thought to use FreeRTOS with the Bluetooth stack with STM32WB family MCU but it appears it is not possible by the STM32CubeMX if you want to build your custom service.Then, I have to use the SEQUENCER but I have no idea how to use it.......
it's returning 0x82.Can someone please help me with this?
The datasheet of the STM32WB5MMG BLE module describes the placement of the module, as well as recommendations for the ground plane on the right side to the module:- The module should be placed in the top left corner- The ground plane should be kept f...
Hi,can someone help me with how to write a value to the server from the client? which API to useThank you,
Hi,I am using STM32WB55CG6 custom board and configured as cliend and trying to connect with server(ESP32 configures as server).When a button is pressed i am connecting to server =============================================================void HAL_GP...