User Activity

I have tried running the BLE_HeartRate application as generated by STM32CubeIDE v1.11.0 which used WB FV 1.15.0. I am running on a custom board (DK board is not available right now) that has a STM32WB5MMG module, the recommended capacitors, and a he...
I am running the above mentioned board about 3 meters away from two gateways, a TTIG and a RAK7258. I made two modifications to the stock End Node application - I modified Commissioning.h with the EUI, etc. for one of the gateways (have tried both)...
Kudos from