STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 241 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4082 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55 Zigbee - Can't report value

Attached is my demo project for the NUCLEO-WB55RG dev kit.I'm trying to report ZCL_TEMP_MEAS_ATTR_MEAS_VAL when the attribute value is changed (button 3 pressed), but according to wireshark, nothing is send.See app_zigbee.c, line 329I can correctly r...

JB1234 by Associate II
  • 3395 Views
  • 2 replies
  • 0 kudos

Stm32wle5jci6

static void SendTxData(void){/* USER CODE BEGIN SendTxData_1 */uint16_t pressure = 0;int16_t temperature = 0;sensor_t sensor_data;UTIL_TIMER_Time_t nextTxIn = 0; #ifdef CAYENNE_LPPuint8_t channel = 0;#elseuint16_t humidity = 0;uint32_t i = 0;int32_t ...

Nani96 by Associate II
  • 1025 Views
  • 0 replies
  • 0 kudos

Resolved! Nucleo-WB15CC : Can't erase all flash sectors

Hi, I am working with a NUCLEO-WB15CC and can't erase all of the 320 KBytes Flash. When using the STM32_Programmer_CLI the following works perfectly fine:STM32_Programmer_CLI.exe -c port=SWD -e [0 55]but withSTM32_Programmer_CLI.exe -c port=SWD -e [0...

hbtest by Associate
  • 2665 Views
  • 1 replies
  • 0 kudos

Resolved! BLE Server Side read Event nevers happens

hi all,I'm working on a STM32WB5MMGHX and I have play with p2p demos and otherI'm trying now to build a Battery service with only a battery level caracteristicI've set the caracteristic as shown belowmy custom app event handler is as folow : void Cus...

oga_0-1698937290193.png
oga by Associate III
  • 1818 Views
  • 1 replies
  • 2 kudos

Going into "OnRxTimeout" with Spreading Factor 12

Hi! So i have a WL55CC MCU that sends a 64 Byte Payload via LoRa to a Nucelo JC1 Board. When I'm sending with a spreading Factor of 7, everything works just fine, but with spreading factor 12 the receiver goes into a timeout mode, although I've set t...

0693W00000HnyExQAJ.png 0693W00000HnyFlQAJ.png 0693W00000HnyGFQAZ.png
GHube.1 by Associate II
  • 1873 Views
  • 2 replies
  • 0 kudos

NUCLEO 32WL and Sigfox: ID and PAC Problems

When setting up the project I go to the ST url to get the ID and PAC from: https://my.st.com/sfxp the zip that is downloaded is corrupted and has a size of 0kb. I have done this procedure hundreds of times so I am sure that the problem comes from the...

mm2k4 by Associate II
  • 9021 Views
  • 18 replies
  • 3 kudos

WIFI Support on STM32W?

Sometimes, if in addition to Bluetooth, WIFI is needed in the development of a product, the third module is used. Does ST plan to include WIFI in the e.g STM32W series in the future?

Slh by Senior
  • 5269 Views
  • 3 replies
  • 5 kudos

STM32WL55JCI7 RF line design

Hello there!I have a request regarding PA matching impedance measurements.We are currently working on the implementation of a VHF pulsar system. Initially, we tested it on the NUCLEO board without incorporating the filtering components (impedance mat...

Resolved! P-NucleoWB55 ST-LINK error STM32 target found

Hi,I am having a problem with my P-NucleoWB55 development board. When using STMCUBEIDE and trying to run the program, I get the following error.STMicroelectronics ST-LINK GDB server. Version 7.4.0Copyright (c) 2023, STMicroelectronics. All rights res...

Sjain by Associate III
  • 1521 Views
  • 1 replies
  • 0 kudos