STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

crc_ctrl.h problem on the STM32WBA6

I'm having the same issue on my NUCLEO-WBA65RI project. This problem specifically occurs when I try to use both X-CUBE-FREERTOS and STM32_WPAN. The project cleanly builds just fine if I only use one or the other, but as soon as I try to include both ...

Resolved! Implementing BLE SPP protocol

I have a requirement to implement the BLE SPP protocol that will eventually be ported to the STM32WB1MCC module. Since I am totally new to BLE, I'd like a recommendation for a place to start. Specifically which demo or eval board and associated softw...

DavePfz by Associate III
  • 889 Views
  • 3 replies
  • 0 kudos

STM32WB1MMC Capabilities Question(s)

This is coming from someone with very limited experience with BLE, so be patient in your response.I have a requirement for a device that will operate as a GATT Server emulating a UART to an external device (IOS or Android). On input from the user, th...

DavePfz by Associate III
  • 483 Views
  • 1 replies
  • 0 kudos

Resolved! Usage fault in WBA6_LinkLayer_BLE_Basic_lib.a

Hi,I'm having an issue with the WBA6_LinkLayer_BLE_Basic_lib.a library on zephyr.The library is found in zephyrproject/modules/hal/stm32/zephyr/blobs/stm32wba/lib directory in zephyr 4.2 (tag v4.2.0 in https://github.com/zephyrproject-rtos/zephyr/tag...

ya by Associate II
  • 1905 Views
  • 8 replies
  • 1 kudos

how to use STM32WB55RG USB as HID device

Hi,I got a NUCLEO-WB55RG board and was trying to program it as a HID device. I have configured the STM32CubeIDE and have uploaded the code to the board. Yet, when I tried connecting the User USB, it unfortunately didn't work. My computer did not reco...

Miooo_0-1765883354678.png Miooo_1-1765883378088.png
Miooo by Associate
  • 445 Views
  • 3 replies
  • 2 kudos

STM32WBA55G-DK1 Auracast Channel issue

Hello,I have created two BIS channels eng and esp, under BIG main group by assigning bis[0] and bis[1] and given left and right channel as the input. At the receiver side, the first channel [0] will perfectly get connect and displays "synced with som...

Sandeep_k by Associate III
  • 942 Views
  • 6 replies
  • 0 kudos