STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Connect BLE on B-U585I-IOT02A Board

Hello,I have flashed the FUS and wireless stack to my B-U585I-IOT02A. However, there are no tutorials on how to set up a simple BLE app with the STBLE Toolbox with this specific board. All of the examples are built for different boards, as listed on ...

Resolved! STM32WL55JC and LoRa

Hi,I have a project based on MIPOT 32001506xxx radio module.The 32001506xxx is a multi-protocol sub-GHz radio module based on STM32WL55JC microcontroller.I need an example to follow to help me use the radio module as a "simple" LoRa modem.Thanks in a...

Resolved! Is STLink-V3MiniE better than STLink-V3SET?

For use with STM32WLE5JC, since I do not need I2C bridge and expandsion, will V3MiniE better than STLink-V3SET?  MiniE higher SWO 24MHz vs 16MHz in slower V3SET.  MiniE is 2 years younger.  TIA

David_ by Senior
  • 3219 Views
  • 3 replies
  • 2 kudos

BLE commands used by STM32WB, explanation needed??

Good evening....I have a few questions:1.  Can someone please explain why with CHAR_PROP_WRITE_WITHOUT_RESP pairing does NOT work but if I change to CHAR_PROP_WRITE pairing works?  I am using Display Only, MITM and no bonding.  Using either one place...

SWenn1_0-1709858454745.png
SWenn.1 by Senior III
  • 1851 Views
  • 1 replies
  • 3 kudos

APP_LOG print float

Hi,I'm usin the seed LoRa-e5 with the BME680.I want send the output of the sensor through uart to the console. The thing is, that most of the output values are float.I'm using the LoRaWAN_End_Node sample as base.Regards,Johannes

JFlor.4 by Associate II
  • 4120 Views
  • 6 replies
  • 0 kudos

APP_LOG print float to serial

Hi, I'm using the APP_LOG function to print data to serial. Here's how i do it:APP_LOG(TS_OFF, VLEVEL_L, "%d,%d,%d,%d,%d,", front_brake_pressure, rear_left_wheel_speed, rear_right_wheel_speed, front_left_wheel_speed, front_right_wheel_speed);APP_LOG(...

FPicc.1 by Senior
  • 1294 Views
  • 1 replies
  • 0 kudos

Queue usage fault

HiI use free-rtos with stm32wb55.I use some queues, they all behave as expected except for one of them (led driver queue).It seemed that some of the messages being sent (to the led driver queue) are ignored or missed.I added a debug code and found ou...

Ofer by Senior
  • 3927 Views
  • 8 replies
  • 5 kudos

Looking to built my own lorawan network server.

Hello everyone,I'm looking to built my own lorawan network. Currently I'm using loriot server. As we need to pay these server. I'm looking to build my own.Looking for the help/guidance on do we need any type of access or permission from these gateway...

Yash_want by Associate II
  • 2534 Views
  • 4 replies
  • 0 kudos

Not able to disable receiving window of L072Z LRWAN1.

Hello everyoneI'm trying to using/operate L072Z LRWAN1 in class c. I'm able to know that node is operating in class c( I'm attaching images below). But i want to disable the receiving window to get faster data rate. In class A I'm getting 20 frames p...

IMG_Class A.jpg IMG_class C.jpg Class C doc.jpg
Yash_want by Associate II
  • 4700 Views
  • 9 replies
  • 3 kudos

Resolved! Reconnection issues using NVM

I am using Zigbee for wireless communication using Zigbee_OnOff_Router_NVM as a reference. The problem I am currently facing is that if I turn off the Router for a long time, it may take about 20 seconds for the data to reach the Coordinator the next...

Born2 by Associate II
  • 1833 Views
  • 2 replies
  • 1 kudos