STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WBA OOB Pairing not working

Hello, I am working with STM32WBA52 and I am using the X-Nucleo-NFC07A1 Tag to try to perform BLE OOB Pairing. From the sparse existent documentation regarding this subject, I have understood that the SecurityParams_t structure had a flag to indicate...

Portilha by Associate II
  • 1752 Views
  • 1 replies
  • 0 kudos

Using the ST-Link V3E on the STM32WL-Nucleo Board

Hello,  I used the onboard ST-Link Debugger of the STM32F401RE to flash/debug external boards. Can I do the same with the Nucleo-STM32WL55JCx Board(using the MIPI10 Connector)? I checked UM2592, and it only gives directions about using an external de...

AElgh by Associate III
  • 3610 Views
  • 8 replies
  • 1 kudos

Resolved! STM32WB55 Shutdown mode

Ciao,I am trying to put my STM32wb55 in shutdown mode and wake it up using 2 external pins.Wake-up sources are on PA0 (active high) and PC12 (active low). Those should be PIN1 and PIN3 wake-up sources.This is the code I use to put the device in shutd...

VM by Associate
  • 5564 Views
  • 2 replies
  • 1 kudos

Resolved! No SubGHz interrupt on STM32WLE

I use a RAK3172 module for a 434 MHz LoRa APRS application but I don´t get a SubGHz interrupt during transmission. The output from my code is the following:APRS DemoApplication version: V1.3.0Radio version: V1.3.0Radio settingsLoRa Bandwidth: 125 kHz...

Kampi by Associate III
  • 6683 Views
  • 6 replies
  • 0 kudos

Disable frame-counter validation in end node

Hello,I have an end-node device based on STM32WLE5CBU6.The end node sends data in every 10 seconds to the gateway.when I reset the End node device the uplink frame count in the end node resets to 0, at this moment the gateway shows a frame counter va...

vishaltechshlok_0-1708691644151.png

Resolved! I cannot see some BLE tabs in CubeMX

Good day, I am working on a custom BLE p2p server using the STM32_WPAN, library. I am working on the STM32WB55 chip with FreeRtos enabled. When I follow the STM32 Bluetooth tutorial on youtube, I realized that many tabs were missing on my setup. Is t...

AMuya.1 by Associate II
  • 3581 Views
  • 4 replies
  • 0 kudos

Looking for information/details on WL55JC1 and B-L072Z LRWAN1.

Hello @STTwo-32  @ST Community Looking for information and details on this.1) Currently I'm using B-L072Z LRWAN1 and I'm looking forward to using WL55JC1, using WL55JC1 CLASS B will increase my data rate?2) Does WL55JC1 support CLASS B and as well as...

Yuvi by Senior
  • 2472 Views
  • 5 replies
  • 5 kudos

SUBSTITUTION LORA GATEWAY WITH A STM32-L476RG

Hi everyone, i would create a LoRaWAN project in which both end-node and gateway are implemented by a NUCLEO-l476rg, because i haven't a gateway. The fictitous gateway is connected locally, with UART, to a python app on my pc, to handle the informati...