STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX for STM32H757I-Eval board

Hello All, I am trying to use STM32H757I-Eval board for one of Development project and need to get one clarification regarding it.I am using Touch GFX Designer Version- 4.24.2, while creating a new project I can see STM32H747l Eval for Board Setup in...

ShivDesh by Associate III
  • 1249 Views
  • 2 replies
  • 0 kudos

Touch GFX and I2C sensors on the same bus

Hi All ,I am doing a projet using STM32f469I disco board with Touch GFX i able to run the Touch GFX GUI properly but when i try to conncet the I2C sensors to the same bus the I2C is always busy with the Touch GFX. hence i am not able to initialize t...

LKade.1 by Associate II
  • 2287 Views
  • 4 replies
  • 0 kudos

Rendering frequency spectrum

Hello,i want to render frequency spectrum FFT in the small area of screen and handle touch in this area. This should be done by some custom widget/container. Can you help me how to do it? Best Regards,Petr

Petr3 by Associate III
  • 6275 Views
  • 14 replies
  • 2 kudos

Import correctly Touch GFX project to Cube IDE

Hi there,I am doing a DIY project based on an STM32F469 disco board. I am using Touch GFX Designer v4.24 and generating the code with it.  The thing is that when I import the project to CubeIDE software, it does not take it as a cproject because it d...

Enekkk_0-1739800619668.png
Enekkk by Associate II
  • 3192 Views
  • 9 replies
  • 0 kudos

X-TouchGFX Addon 4.25?

I am evaluating the MP line of processors and want to use TouchGFX. The current version of TouchGFX is 4.25.0 put the MPU addon is 4.24.0 and won't install with 4.25.0.  Is an updated MPU addon coming out soon?

Resolved! Artifacts in a blank GUI

Hello, I am working on a project that includes HTTPS communication, peripheral communication via LIN, and a graphical user interface. I am using the STM32H745I_DISCO board. I have already tested and successfully implemented the HTTPS and LIN parts.Ye...

RafaelS by Associate III
  • 1488 Views
  • 2 replies
  • 2 kudos