STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! CubeMX 5.0.1 Empty hal_conf file on 32F746DISCOVERY demo

I am attempting to ​setup the TouchGFX on a 32F746DISCOVERY Board with CubeMX and SW4STM32.When I create the Board project in CubeMX, the stm32f7xx_hal_conf is empty. I would have expected that the Peripherals would have some initialization code setu...

MEder by Associate III
  • 1009 Views
  • 3 replies
  • 0 kudos

Setting a low-level timer

Hi,What method would you recommed to set up a low-level timer on my board? HAL libraries ? Configuring directly the registers ? Something else? EDIT : I'm asking cause I'd like to measure the time it takes to perform a certain action (say color the b...

GMeur by Senior II
  • 1212 Views
  • 2 replies
  • 0 kudos

STM32F4 Discovery + STemWin + ILI9341 SPI

Hello, as the Question says, I'm trying to run STemWin into STM32F4 Discovery board. It compiles well, but does not show anything. I think the LCD initializes, but after that, It does not work anymore. I'm using ATollic Truestudio and an Arduino LCD ...

GCerv by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

what do you use to program STM32F769I-Discovery

I downloaded CubeMX 7 I thought it was program like Cube Mx 5, instead it had bunch of example files. When I try to generate code in Touch GFX, the right upper corner nothing happens.So what do you use to get the working TFT and bunch of other things...

MNapi by Senior III
  • 1651 Views
  • 7 replies
  • 0 kudos