cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Discovery + STemWin + ILI9341 SPI

GCerv
Associate

Hello, as the Question says, I'm trying to run STemWin into STM32F4 Discovery board. It compiles well, but does not show anything. I think the LCD initializes, but after that, It does not work anymore. I'm using ATollic Truestudio and an Arduino LCD with an ILI9341 by SPI. The library I've used is: https://github.com/martnak/STM32-ILI9341

It works perfectly fine with this set up.

Since CubeMx does not support STemWin with this board, I build the project by myself. I think the problem is the LCDConf file.

I do not use RTOS and I don't get any error, the code get just stucked when I use "GUI_DispStringHCenterAt".

Can somebody help me?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Mon2
Senior III

Hi. Which STM32F4 Discovery kit exactly are you using?

If you have the STM32F429I-DISC1, you can review the following thread:

https://community.st.com/s/question/0D50X0000A4pPgPSQU/stm32f2429-disc1-configuration-with-touchgfx-cubemx-50

Proven procedure for this kit, using TouchGFX (not STemWin) but can use IAR or SW4STM32 compiler with working GUI tools including touch.