STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

4.11 Can not create/open project

I check the log, it will pop this error:System.ArgumentException: 已添加了具有相�?�键的项。(An item with the same key has already been added)  在 System.ThrowHelper.ThrowArgumentException(ExceptionResource resource)  在 System.Collections.Generic.Dictionary`2.Ins...

DJin.3 by Associate
  • 894 Views
  • 1 replies
  • 0 kudos

TouchGFX 4.10.0 and MSVS 2019

I am new to coding in touchgfx. i am using touchgfx 4.10.0 version and microsoft visual studio 2019. Depends on version, is there any difference in coding method?I followed one button example, which was already available in touchgfx examples. I devel...

YK.10 by Associate II
  • 996 Views
  • 1 replies
  • 0 kudos

CubeMX 5.1.0 GFX Simulator setup

There is a new feature in CubeMX,  the GFXSimulator.  ​If I import settings the configuration then gets populated with the Simulator settings.  Seems backwards, and produces Clock errors.I copied the Configuration to the simulator settings. Is the fo...

MEder by Associate III
  • 3157 Views
  • 6 replies
  • 0 kudos

Flicker appears when configure LCDConf to GUICC_M888

I created a project based on STM32Cube_FW_F7_V1.15.0, using the STM32746G-Discovery project. I have my own hardware using STM32F767 with external SDRAM at 16bit bus, and Nor flash via QSPI. My hardware has a 10 inches LCD with 24bpp RGB interface and...

jcaza by Associate
  • 852 Views
  • 0 replies
  • 0 kudos

Resolved! STM32 BSP Documentation?

Posted on January 12, 2018 at 03:14I've just purchased an STM32F469 Discovery development board.  I've got the latest version of STM32Cube and able to build and run various examples on the board.  What I'm not finding is some decent documentation fo...

Touch GFX : error during code generation

Hi,I'm using touch GFX designer 4.10 to make a simple application on the STM32F429 discovery.I opened Touch GFX designer, I create my first application based on the STM32F429 discovery, I try to run on simulator, on target and generate the code ==> i...

JEN by Associate II
  • 1188 Views
  • 1 replies
  • 0 kudos

Screen redraw

Hi, I have a problem redrawing the screen after changing the content. I am using FreeRTOS and TouchGFX runs in one task, and the modifications runs from a different task.The constructor of the screen adds all drawables to the screen object. But they ...

0690X000009YNs5QAG.jpg 0690X000009YNsAQAW.jpg 0690X000009YNsFQAW.jpg
kvl by Associate II
  • 2588 Views
  • 2 replies
  • 0 kudos