STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TouchGFX Academy launch announcement!

Dear Community, We're excited to announce the creation of the TouchGFX Academy! The TouchGFX Academy is a new place to learn TouchGFX with concrete examples and to find answers to your questions when developing your UI. It includes tutorials of cour...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32 STemWin and Interrupt Problem

Posted on April 10, 2015 at 16:52 I'm using STM32F407ZGT6 with SSD1963 LCD controller and 800x480 TFT panel. I'm not using OS. It's working with STemWin.  But when I used any interrupt, code execution stops at somewhere in emWin.  I moved WM_Exec() ...

ilmete27 by Associate
  • 420 Views
  • 1 replies
  • 0 kudos

STemWin Hide Desktop Window of Second layer

Posted on April 08, 2015 at 21:12Hello, I'm using STemWin, and I'm facing a problem. I'm using the Window Manager, and two layers. But I only want to use the Window Manager in one layer (background layer), but not on the foreground layer. Is this po...

fb2 by Associate II
  • 309 Views
  • 0 replies
  • 0 kudos

32F429IDISCOVERY LCD ILI9341 driver

Posted on March 19, 2015 at 15:17Hi,I would like to ask if anyone has successfully changed the setting of the ILI9341 driver to little endian...I have data in this format but in default I have to send over SPI high byte first and low byte after that...

32F429IDISCOVERY LCD ILI9341 driver

Posted on March 18, 2015 at 01:32Hi,I would like to ask if anyone has successfully changed the setting of the ILI9341 driver to little endian...I have data in this format but in default I have to send over SPI high byte first and low byte after that...

STemWin VNC server compatibility

Posted on March 05, 2015 at 12:17HelloI am trying to use the STemWin library as a VNC server with a STM32F429 microcontroller.It works fine as long as I use a VNC client running on windows, for example UltraVNC.I have tested several VNC clients for ...

DCMI: pixel clock issues

Posted on February 18, 2015 at 12:59Hi GuysI' trying to get an image with DCMI module. So, I set up the camera sensor for a square test pattern (a grid of 16 white pixels and 16 black pixels). I get the data with the DMA and the grid obteined was 2x...

How to enable multi ADC using STM32F407ZG?

Posted on February 22, 2015 at 06:43I am using 2 ADC's ,1. for Touch Panel (ADC1)2. another for getting input from potentiometer (ADC3)Earlier Touch Panel program was working fine, when I implemented by initializing ADC3, there is a conflict, so the...

dhinesh by Associate
  • 560 Views
  • 3 replies
  • 0 kudos