STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TouchGFX Academy launch announcement!

Dear Community, We're excited to announce the creation of the TouchGFX Academy! The TouchGFX Academy is a new place to learn TouchGFX with concrete examples and to find answers to your questions when developing your UI. It includes tutorials of cour...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

About the STemWin of the STM32F4 Discovery.

Posted on March 26, 2016 at 18:09I used the STemWin_SampleDemo from the STM32F4 Discovery SDK to run my program. I find out that if I put WM into menu controls, when I delete(WM_DeleteWindow) the menu widget, that MCU will appear HardFault_Handler. ...

yaomei65 by Associate
  • 280 Views
  • 0 replies
  • 0 kudos

Is this a bug in the HAL DCMI driver?

Posted on March 07, 2016 at 16:52 This is from the 1.0 driver. (I'm downloading the next version but it is going. Real. Slow.) From STM32Cube\Repository\STM32Cube_FW_F4_V1.0\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_dcmi.c ...

hbarta2 by Associate III
  • 345 Views
  • 2 replies
  • 0 kudos

stm32f103 and winstar TFT display problem

Posted on March 09, 2016 at 14:24Hi all, I have problem with displaying any data at WF57STIACDNN0 TFT display. This is a TFT display with ST7511U driver. In my SW driver I successfully pass the display initialization procedure - I see some randomize...

Rotation of STM32F429I-Disco LCD

Posted on February 11, 2016 at 21:18So I've been through the HAL, the CubeF4, and the StdPeriph library. There are many functions to do many things to the LCD but I cannot for the life of me find one to rotate the LCD or initialize it in with a land...

ejanuska by Associate II
  • 1242 Views
  • 2 replies
  • 0 kudos

about STemWin Window Manager

Posted on February 25, 2016 at 08:51Hello, I using STemWin, but I don't want to use window manager when I call GUI_Init() function and get GUI free bytes(GUI_ALLOC_GetNumFreeBytes()) it's always reduced 2.5K for GUI's memory (I see emwin user guile,...

yaomei65 by Associate
  • 305 Views
  • 0 replies
  • 0 kudos

stm32f756 dcmi - no dcmi interrupts

Posted on February 15, 2016 at 11:23Hi all Problem exists in custom board with adapted BSP from stm32f7 discovery. For ov2640 sensor I use component library from stm32cubef2.If initiate a camera with any resolution and begin transferring getting onl...

STemWin Library problem while Rotating LCD

Posted on February 12, 2016 at 13:38Hello, I am currently working with STM32F439ZI microcontroller and interfaced SPI LCD having 144x128 resolution with MCU. STemWin library is used to run my GUI on LCD. Currently I am facing issue of how to rotate ...

nipam by Associate
  • 298 Views
  • 0 replies
  • 0 kudos

FSMC timing calculation

Posted on February 08, 2016 at 14:40hello, I want to interface SSD1289 lcd controller to stm32f103zet6 micro controller. I'm trying to understand the FSMC timing computations but to no avail. I referred to application note and found the following. C...

0690X00000605LNQAY.png 0690X00000605LSQAY.png

SDIO transfers gets stuck

Posted on September 14, 2014 at 13:13Hi everyone. I'm having trouble writing images from a camera to a microSD card on my STM32F4 Discovery board. The SD writes keep getting stuck in the HAL function, SD_DMA_RxCplt(). I'm using FAT_FS, so even thoug...