STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Error when creating applications

When I try to create a project for a Discovery Kit or open the online application in TouchGFX Designer, the "Downloading Application Template" and "Downloading GUI" slowly reach 100% and then this error screen is displayed:/*Sorry - something unexpec...

Henrik C by Associate II
  • 966 Views
  • 1 replies
  • 0 kudos

STemWin Alpha channel

I'm using an stm32f769 on an ARGB8888 system.I'm creating a bitmap image in RAM from a JPEG using the hardware decoder. This is decode process does NOT set the alpha byte to 0xff so the GUI_DrawBitmap function using the GUI_DRAW_BMP8888 method doesn...

STM32CubeIDE with TouchGFX 4.12.3

I have several errors while generating my code. A few errors i am able to solve with excluding the simulator files from my project. But now i have a new error with an undifened reference. ../TouchGFX/generated/fonts/src/GeneratedFont.cpp:12: undefine...

0690X00000AqKciQAF.png
Fab_0815 by Associate III
  • 2307 Views
  • 8 replies
  • 1 kudos

New versions on stm32f769i-disco

I tried to create a project with the new versions of cubeide and touchgfx. After disabling the watchdogs and SDMMC2, and programming with the st-link utility, it ran in the debugger. The output isn't what I created in touchgfx.I noticed that this l...

0690X00000AqR8fQAF.jpg
TWebs.1 by Associate III
  • 2004 Views
  • 6 replies
  • 0 kudos

Example code RTOS + HDMI

Hi,I've been looking into the STM32373C-EVAL and the STM32CubeF3 since I need to build a prototype that includes RTOS and HDMI output. The board includes a LCD display and 2 HDMI outputs. The STM32CubeF3 includes some FreeRTOS examples and some LCD e...

Flux by Associate
  • 1344 Views
  • 1 replies
  • 0 kudos

library-function access on packed text structures

We have discovered that it seems that TouchGfx library functions like "InternalFlashFont::getPixelData" accesses the packed (2 Bytes) text ressources with a unpacked (4 Bytes) access.This ends up in an misaligned HardFault.What goes wrong here?

MHase by Associate II
  • 1004 Views
  • 1 replies
  • 0 kudos