STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Linker errors and "Run target" fails

hi everyone,i wanted to create a project with touchGFX but there are errors, i just create the graphic interface, i didn't add any code!even though when i tried to upload to my card an example it said error too!how can i resolve this? 

0690X00000BwBSfQAN.png 0690X00000BwBRIQA3.png 0690X00000BwBRDQA3.png 0690X00000BwBR8QAN.png
idrissmc by Associate III
  • 10010 Views
  • 43 replies
  • 0 kudos

Is there an inbuilt language translator for TouchGFX?

Is there an inbuilt language translator for TouchGFX? For example, if i create an application in english but want an option for other languages as selected by user , do i need to create the same one again or there is an option for auto generated code...

biki by Associate II
  • 1286 Views
  • 1 replies
  • 0 kudos

Resolved! Different display for the STM32F746 DISCO board

Has anyone used a different display with this development board. I am trying to use a Newhaven 320 x 240 display with this board. I have removed the display and made an adapter board as the Newhaven has a 54 pin connector and the DISCO board has a 40...

TouchGFX example on "non ST produced" STM32 development board like HOTMCU SOM-STM32429IG to demonstrate CUBEMX TouchGFX CubeIDE integration

Hi I have spent a long time trying to get a working example going on a 3rd party STM32 development board, to try and learn the difficulties in getting a project up and going from scratch.The ST examples are awesome and work beautifully on the off the...

GOmon.1 by Associate III
  • 2085 Views
  • 1 replies
  • 0 kudos

Swipe in 2 dimensions

I want to create something that is almost a 2D swipe container. but in reality I think the best solution is several screens, each with swipe containers, and a vertical swipe on any one will transition North/South to the next page.Is there documen...

getTypedText() access error

Hello,I'm trying to retrieve the text string of a textarea widget with the function getTypedText() but I get an access error. No wildcards are used in the textArea2, the propery "Text"is just filled in with a short text in the designer.

0690X000006DcnzQAC.png
GMeur by Senior II
  • 1393 Views
  • 5 replies
  • 0 kudos