cancel
Showing results for 
Search instead for 
Did you mean: 

ApplicationTemplate.touchgfx.part cannot be open. Please help me!

JPark.14
Associate III

Dear all,

After I made a project with CubeMX 5.5 and checked a Graphics Application to use TouchGFX. Other all settings was good, I think. And then I did "GENERATE CODE" and I got ApplicationTemplate.touchgfx.part file. But this file cannot be open with TouchGFX 4.13.

Error Message is like "Object reference not set to an instance of an object".

( I translated it in English.)

Could you let me know about the reason and give me a right solution?

(The attached is a .part file.)

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Michael K
Senior III

I was able to open the .part file with TouchGFX 1.13.

Does it work if you open TouchGFX designer first and then click File->Open and open the .part file that way? Can you open any other .part files?

Embedded UI/UX Consulting: cadenza.design
JPark.14
Associate III

Thank you for your reply, Michael.

No,.. I tried to open it by the right steps that you mentioned but I failed to open it. I think the .part file extraced from CubeMX code generation is not perpect. Actually I filled some items by refering to other .part or touchgfx file and I could open it. Of course the final file is so different from the original one.

I will try other things and post some question if anything strange. And please let me know if there are other things that I have to know about this matters.

Thank you~!!