Associate II
February 10, 2020
Question
Application Fails when Framebuffer stored into an external RAM
- February 10, 2020
- 2 replies
- 1197 views
The STM32CUbIde dont support TouchGFX yet to build a project based on STM32L4R9AII6, so I build my own project . I faced a very serious problem when I try to put a FramBuffer into an external RAM configured as memorymap (OCTOSPI) .
When I do this a vertical lines are displayed (see attached image) and the image quality is degraded
Please can you give me a possible solutions.
Thank you.