STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Cube IDE Debugging -- Proper Sequence?

Hi -- just wondering if anyone has tried importing a project generated by the Designer to the Cube IDE, and then had any success running it using the GDB debugger on either a 746 or 769 Discovery board? Everything seems to build fine in Designer and ...

Chandler by Associate II
  • 16923 Views
  • 24 replies
  • 0 kudos

DSI 2-lane or 4-lane?

Hey everyone!I'm not sure if this is the right forum to ask HW related questions but here goes:I've found a nice big 4-lane DSI display that I would like to hook up to an STM32F7xxx.My issue is that as far as I can see the STM32 parts only supports 2...

HP by Senior III
  • 3002 Views
  • 1 replies
  • 1 kudos

TouchGFX generation in STM32 CubeMX

I have the library installed, the application selected, and the selection under Additional Software X-CUBE-TOUCHGFX... selected and enabled. However, when I hit Generate Code, none of the TouchGFX folders are created, and the build fails with missing...

Resolved! Best way to implement Screen timeout?

Hello,I am trying to implement a basic screen timeout where the current screen is changed to the startup screen after a set time.The timeout itself is straightfoward to implement using a tickcounter. However, the problem I am facing is resetting this...

SKILA by Associate II
  • 2376 Views
  • 5 replies
  • 0 kudos

Speed up compile time in STM32CubeIDE

Hi,Is there a way to compile the firmware using GCC in different computers or in a faster server available in local network?I am using STM32CubeIDE, GCC, TouchGFX and my compile time is increasing as the code sizes increases too. Now I take about 5 m...

eng23 by Senior
  • 5892 Views
  • 9 replies
  • 0 kudos

Internal Frame buffer handling by user

Hi,I am using STM32L4R9 to implement graphics using TouchGFX. And i am using 390x390 Amoled Display.I have a requirement to display time always on the display whenever the device not being used , but with very less power consumption.So do you guys an...

Bala1 by Associate II
  • 1461 Views
  • 3 replies
  • 0 kudos

Resolved! Using CPP Exceptions in touchgfx application

Hi,Our embedded application heavily uses CPP exceptions. CPP exception support is enabled in IAR under Options -> cpp options -> Enable exceptions . I am trying to integrate the touchgfx library with our embedded application based on STM32H743I MCU....

STang.1 by Associate II
  • 3807 Views
  • 9 replies
  • 0 kudos