STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Statically allocate N number of containers?

Hello,I want the user to be able to configure UI. There is configuration view (settings menu) which will add N number of containers to another view.Currently there is no customization, only fixed number of containers are allocated.parameterContainer ...

Tuoman by Senior II
  • 2080 Views
  • 7 replies
  • 0 kudos

Resolved! Is there documentation on TouchGFX on how it works?

I see the on-line tutotrial-style documentation. I see the doxygen-generated details. Is there any documentation that describes how it actually works? What is the architecture? What calls what? What are the operations inside the binary library?The re...

Resolved! How to re-use some screens from previous project ?

Hi.Is it possible to re-use some of the screens of previously developed TouchGFX project ?I have tried the option of importing the GUI but it overwrites my current project.Please share your thoughts or suggestions.Regards,Shree

Shree by Associate II
  • 1300 Views
  • 3 replies
  • 0 kudos

STM32H7 DCMI or OV9655 configuration issue?

Hi everybody,ST has an example for OV9655 from STM32Cube_FW_H7_V1.5.0We use the configuration for VGA mode, without any change. Most of the time image good and clear. Just sometime, when reset the board, a noise picture appears as below. Once noise p...

Dat Tran by Senior II
  • 1340 Views
  • 1 replies
  • 0 kudos

Resolved! Tutorial for CubeIDE with QuadSPI

I found out today that my project was not properly configured. So i did run out of flash memory.By comparing with a Designer project I found out how to change the FLASH.ld file to use QuadSPI and some other things that were different in the Designer ...

Hello guys, I have a 5" CTP display (SEE ATTACHED) and like to know if i can use this with only STM MCU or i need additional LCD driver like SSD1963 for my ongoing IoT device project ?

What are the requirements when i selecting MCU for this display ? My end goal would be the following:  *Cheap as possible (however not make the display quality worst/slow) *This IoT device will get some information from a API server, and run some ani...

Ikiss.1 by Associate II
  • 2364 Views
  • 4 replies
  • 0 kudos