STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

File explorer example using touchGFX

Is there any file explorer example to show the content of SD Card using touchGFX?Currently I'm designing HMI for Industrial automation, Where I need to provide optionto select/create a file for storing data acquired by some of the input channels.Kind...

rangam by Associate
  • 2054 Views
  • 3 replies
  • 0 kudos

Region `FLASH' overflowed for external flash

Hello, region `FLASH' overflowed by 424008 bytes but i didn't added much image. I am using 128 Mb N25Q128A13EF840E QSPI flash. I just wanted to confirm how much QSPI is assigned.I can see below settings for QSPI.I want to know that Where should I che...

0693W000001stCiQAI.jpg

How can I make 90deg keyboard on 272x480 screen?

Hello,I saw keyboard example but all example for 180deg display orientation. I am using 480x272 LCD but screen orientation is 90deg than ı have 272x480 screen. In examples keyboard is on 320x240. How can I use this examples or Any solution avaiable ?...

My touchscreen is not working properly

Hi All.I have my own development board on STM32.TouchGfx 4.13.0 is ported to it.Displays box, button, scrollbox and text.The coordinates of the touchscreen I pass tobool STM32TouchController::sampleTouch(int32_t& x, int32_t& y) {   if(touchDa...

0693W000000VSTcQAO.jpg
ANapa by Associate III
  • 6559 Views
  • 17 replies
  • 0 kudos

Resolved! Imperfect animation with TouchGSX

Hello,i'm trying to execute a simple animation with TouchGFX. I'm using the Texture Mapper image, and i want to reproduce a spin of that image. As you can see in this video it was succesfully done. However, there is an extra random flashing.I'm using...

AMerc.4 by Senior
  • 1220 Views
  • 1 replies
  • 0 kudos