User Activity

Hello,I know this has been discussed before and the problem is usually related to the font type used.My problem is that there are certain ligatures in Arabic that don't seem to work when running the TouchGFX simulator. For instance, جهاز renders ok b...
Hello,I have a general question about DMA which I am currently using to transfer a LUT in the memory to control PWM output.The LUT changes periodically and at the moment the DMA is triggered with a timer. What I would like to know if it is safe to ch...
Hello,I am having a problem with CubeMX failing to load a project and not giving any description of what the error is. (See image)I started the exe using java to get more insight and I get this error2021-02-23 10:57:51,490 [ERROR] ThirdPartyModel:101...
Hello,I have recently decided to try upgrading a project I have originally generated using CubeMx 5.6 and designed using TouchGFX 4.13 to CubeMx 6.1 and TouchGFX 4.16. After some teething problems, I have managed to get it working and running on my c...
Hello,I have tried to edit the text.xlsx file for translation purposes and for some reason after accessing the file with excel, generating the code no longer works. This is the message I get nowGenerate Code Generate Done Generate Ass...