STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Segmentation fault in screen transition

The application has 3 screens(say A, B , and C). Here is a summary of a behavior that is showing up in the simulator:Transition from A --> B, B-->A work fineTransition from A --> C, C-->A work fineTransition from B-->C works fineHOWEVER, C-->B gives ...

RMoha.2 by Associate II
  • 1198 Views
  • 1 replies
  • 0 kudos

touchgfx does not swap the framebuffer

the project from designer is running correctlythen,i open the .ioc with cubeMX, select the option <generate peripheral intialization as a pair of .c/.h files per periphreal >,and re-generated the code , in running, the screen display nothing and chec...

zaric by Associate II
  • 3411 Views
  • 8 replies
  • 0 kudos

TouchGFX, rendering bug with big glyphs

HiI'm using a big font size (let's say 400), and glyphs are not refreshed correctly when partially invalidated. It's like the wrong part of the glyph data is copied to the framebuffer.I've attached a minimal project that shows the bug. All is done th...

Gom by Associate II
  • 2715 Views
  • 5 replies
  • 0 kudos

Program crashed when I declare a array of Custom Container and add it to scrollableContainer in a constructor.

I want to display a list of Custom Container in a scrollableContainer .So I write the code like blow.//declare in public std::vector <menuDisplayContent> menuDisplayContanier;   /*--------------------------------------------------------------------*/...

Wrend.1 by Senior
  • 1294 Views
  • 5 replies
  • 0 kudos

STM32 Touchgfx; no Stm32 target found error.

I have STM32H745I- DISCO evaluation board. First, i used Touchgfx (V.4.14.0) and STM32H750B-DK for application template. After a couple of change and run, suddenly "run target" started to give an error and white screen came up on the LCD. It's saying...

FTumer by Associate
  • 1758 Views
  • 2 replies
  • 1 kudos