cancel
Showing results for 
Search instead for 
Did you mean: 

I cant detect touch on STM32f746. I'm using stmpe811 for touch controller

q123w123e123qweqwe
Associate III

Hello,

I'm working on a project an using STM32F746 and STMPE811 for touch controller. I did initializations and everything but no metter hjow much try I can't detect touch. Also I con't do debugging step by step because my code always goes into TIM6_DAC_IRQHandler() funtion. and come back to where it was. it do not go to next line(only if I try debug step by step). So can anyone help me with these issues?

Thank you.

bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y)
{
    if (tsDriver)
    {
        //In here DetectTouch's value is always 0x80060c3 Idk why
        if (tsDriver->DetectTouch(TS_I2C_ADDRESS))
        {
            /* Get each touch coordinates */
            tsDriver->GetXY(TS_I2C_ADDRESS, (uint16_t*)&y, (uint16_t*)&x);
            return true;
        }
    }
    return false;
}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Martin KJELDSEN
Chief III

How did you create this project? The code looks like something we wrote for the Touch Controller in the latest application template.

/Martin

I’ve got it from template project for STM32F429 discovery. Because as I said I’m using stmpe811. So integrated it to stm32f746 custom project. Was it a bad idea?