STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Hey everyone! i am trying to run any template program from touchGFX on the STM32F7691-Discovery but this error message shows up on the log file:

 make -f ../gcc/Makefile -j8 flash    Converting images    Linking TouchGFX/build/bin/target.elf    Producing additional output formats...     target.hex  - Combined internal+external hex     intflash.elf - Internal flash, elf debug     intflash.hex ...

'RAM' overflow and 'FLASH' overflow STM32F7508-DK

I followed the tutorial online. I started a cubeIDE project and used the ST32F7508 template to set up my project. I followed the online setup help to setup. Then I created a touchGFX from the file but when i go to build I keep getting this error and ...

DMeis.1 by Associate III
  • 3670 Views
  • 8 replies
  • 0 kudos

STM32F469I-DISCO. Screen using a custom container made-up for 16 checkbox, work in simulator but not in the hardware board.

Hi,I'm developing an application using touchGFX Designer Version: 4.13.0, all is working correctly when you run Simulator in touchGFXDesingner tool, but when flashing in disco board the screen is fridge and I have to reset the system, again and again...

DCMI capturing issue on NUCLEO 144 STM32H745

Hello everyone!I'm developing a firmware to capture video frame from a thermal camera.I was using a F4 chip.But due to the resolution and fps , I had to migrate to H7 (STM32H745).And now I'm having strage problems with the dcmi.The dcmi start sucessf...

Jvela.11 by Associate II
  • 1096 Views
  • 1 replies
  • 0 kudos

Resolved! What is the best STM LCD board for monitoring?

Hello, want to make a full analog synthesizer with just a screen for monitoring. We would therefore need a lot of ADC and GPIO pins to know the potentiometer value. We have seen STM boards with integrated LCDs, it would help us enormously but I canno...

FAlba.1 by Associate
  • 1053 Views
  • 2 replies
  • 0 kudos

STM32H750 using LTDC as VGA output

My reading reference manual it seemed possible at first. I've set back/front porches and sync values in IDE, but it seems I can't anywhere set refresh rate/pixel time. Does this mean that it can't be done?

Slina by Associate III
  • 2024 Views
  • 4 replies
  • 0 kudos