STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Posible bug in Touchgfx Keyboard ?

Hey, I'm working on custom board Touchgfx project and I'm using Keyboard widget for text input. During testing I found out that keyboard Cancel event is not working properly.Description of problem: When i click and hold on one of keys and drag out of...

JLakn by Associate II
  • 3885 Views
  • 5 replies
  • 0 kudos

how to set up LTDC Hsync,Vsync and porch value???

hi.​I am using STM32F767 to control RGB TFT LCD. Data is output on the screen with TouchGFX.But sometimes the screen momentarily breaks for a very short period of time and then comes back.​When I changed the porch value of LTDC, the cycle of symptoms...

0693W000005ABMNQA4.png
ikassma by Senior
  • 3200 Views
  • 3 replies
  • 0 kudos

Resolved! X-NUCLEO-GFX01M1 and NUCLEO-F446RE: External Loader

I'm trying to port the STM32G071 NUCLEO DEMO downloaded via TouchGFX Designer 4.15.0 to the NUCLEO-F446RE.In order to use the external SPI Flash memory on the X-NUCLEO-GFX01M1 I need the external loder for the STM32F4 processor.The project downloaded...

ALomb by Senior
  • 2091 Views
  • 1 replies
  • 0 kudos

Problem adding a new virtual function to Touchgfx stopsSTMCubeIDE compiler if I try to include definition in relevant screen hpp file.

Everything looks ok and seems the same as all examples however trying to declare any new virtual functions gives me an error so I guess I'm doing something wrong. See code extracts below :-Code extract from Screen1ViewBase :-class Screen1ViewBase : p...

Brotech by Associate
  • 2411 Views
  • 2 replies
  • 0 kudos

TouchGFX bootloader, dfu posibilities

Hi, I have been building on a demo STM32F746g-DISCO touchgfx application for a little while now.My next thing I want to acheive is software update. I realised that the application do not fit in the internal flash.So I am thinking about my options. Ei...

RPipi.1 by Associate II
  • 1663 Views
  • 1 replies
  • 0 kudos